Hello. One of my customer has told me if it is possible to charge an small battery (15mAh) by Wireless power. The problem is that the area that I can use for everything is 15mmx15mm. I have being reading about Tesla power charging (you (TI) will have the BQ5000 series prepared for the 1st semester 2011, Induction charging etc, but the smaller coils need I have seen are 35 mm diameter.
Anyone knows any possibility to get power by wireless into a 15x15 mm board? I think it is not possible, but I am not sure.
Thanks
Javier