Hi Expert
Last week I ask a E2E question that "can BQ25700A support 8A output". Thanks for your reply! becasue I can't open that question website, so I create this question!
Following is the project information: NB project for 20V/5A input (type-C), vsys need to support 100W ( 3S 12.6V/7.9A or 4S 16.8V/ 5.9A )
I saw that Joel answer that "there is a minimum of 8mOhm that can be applied as the ACN/ACP sense resistor"
I want to ask that " do we need to take care about what items when we design the circuit?"
How large the buck-boost MOSFET and inductor saturation current need to reserve?
Thanks!
BR
Bruce