Part Number: TPS62822
Hi, Team,
In the datasheet 9.2.2, it is recommended that the current value of the FB circuit is around 5μA. For 1.8 V, a customer would like to use the below value. Since the IC inflow current of FB is described as 10 nA, it means that the output voltage drops by about 0.2%. The resistance value of the capacitor of CNF also becomes 1/10, so they plans to change capacitor 120PF ⇒ 1000PF. If there any concern with the above setting?
FB/GND 10kohm
FB/Vout 20kohm
Best Regards,
Satoshi Yone