Part Number: BQ27510-G3
Hello,
After performing the golden image, i check the SOC and the TTE on the product
Every 10 sec, I read the TTE and SOC.
During the discharge, the TTE is acceptable and follow a straight line during 8 hours. The TTE decrease every minute. It is OK
But for the last 5 minutes the TTE decrease very slowly.
TTE = 5 during 1min30sec
TTE = 4 during 1min30sec
TTE = 3 during 2min0sec
TTE = 2 during 4min10sec
TTE = 1 during 6min20sec
Please find curve for the voltage, current, TTE and SOC during charge and discharge
Please find the log during the last 5 minutes
13/09/2018 20:03
Temp Voltage FCC Current TTE_Coef_1 Cycles SOC
315 3392 7062 -853 5 14 2 TTE = 5 during 1min30sec
315 3392 7062 -853 5 14 2
315 3391 7062 -853 5 14 2
315 3391 7062 -853 5 14 2
315 3390 7062 -853 5 14 1
315 3390 7062 -853 5 14 1
315 3390 7062 -853 5 14 1
315 3390 7062 -853 5 14 1
315 3390 7062 -854 5 14 1
315 3390 7062 -854 4 14 1 TTE = 4 during 1min30sec
315 3389 7062 -854 4 14 1
315 3389 7062 -854 4 14 1
315 3389 7062 -854 4 14 1
315 3388 7062 -854 4 14 1
315 3387 7062 -854 4 14 1
315 3388 7062 -854 4 14 1
315 3387 7062 -854 4 14 1
315 3387 7062 -854 4 14 1
315 3387 7062 -854 3 14 1 TTE = 3 during 2min0sec
315 3386 7062 -854 3 14 1
315 3386 7062 -855 3 14 1
315 3386 7062 -855 3 14 1
315 3385 7062 -855 3 14 1
315 3385 7062 -855 3 14 1
315 3384 7062 -855 3 14 1
315 3384 7062 -855 3 14 1
315 3384 7062 -855 3 14 1
315 3383 7062 -855 3 14 1
315 3383 7062 -855 3 14 1
315 3382 7062 -855 3 14 1
315 3382 7062 -855 2 14 1 TTE = 2 during 4min10sec
315 3382 7062 -855 2 14 1
315 3381 7062 -856 2 14 1
315 3381 7062 -856 2 14 1
315 3381 7062 -856 2 14 1
315 3380 7062 -856 2 14 1
315 3379 7062 -856 2 14 1
315 3379 7062 -856 2 14 1
315 3378 7062 -856 2 14 1
315 3378 7062 -856 2 14 1
315 3378 7062 -857 2 14 1
315 3377 7062 -857 2 14 1
315 3376 7062 -857 2 14 1
315 3377 7062 -857 2 14 1
315 3375 7062 -857 2 14 1
315 3375 7062 -857 2 14 1
315 3375 7062 -857 2 14 1
315 3374 7062 -857 2 14 1
315 3368 7062 -905 2 14 1
315 3373 7062 -857 2 14 1
315 3372 7062 -858 2 14 1
315 3372 7062 -858 2 14 1
315 3371 7062 -858 2 14 1
315 3370 7062 -858 2 14 1
315 3369 7062 -858 2 14 1
315 3369 7062 -858 1 14 1 TTE = 1 during 6min20sec
315 3369 7062 -859 1 14 1
315 3368 7062 -858 1 14 1
315 3367 7062 -859 1 14 1
315 3366 7062 -859 1 14 1
315 3366 7062 -899 1 14 1
315 3365 7062 -860 1 14 1
315 3364 7062 -860 1 14 1
315 3363 7062 -860 1 14 1
315 3362 7062 -861 1 14 1
315 3361 7062 -861 1 14 1
315 3361 7062 -861 1 14 1
315 3359 7062 -861 1 14 1
315 3358 7062 -861 1 14 1
315 3357 7062 -861 1 14 1
315 3357 7062 -861 1 14 1
315 3356 7062 -862 1 14 1
315 3355 7062 -862 1 14 1
315 3354 7062 -863 1 14 1
315 3353 7062 -863 1 14 1
315 3352 7062 -863 1 14 1
315 3351 7062 -863 1 14 1
315 3350 7062 -864 1 14 1
315 3348 7062 -864 1 14 1
315 3347 7062 -864 1 14 1
315 3346 7062 -864 1 14 1
315 3345 7062 -865 1 14 1
315 3344 7062 -864 1 14 1
315 3342 7062 -865 1 14 1
316 3341 7062 -865 1 14 1
315 3340 7062 -866 1 14 1
315 3338 7062 -867 1 14 1
316 3337 7062 -867 1 14 1
316 3336 7062 -868 1 14 1
316 3334 7062 -867 1 14 1
316 3333 7062 -868 1 14 1
316 3332 7062 -868 1 14 1
316 3330 7062 -869 1 14 1
316 3330 7062 -859 0 14 1
316 3328 7062 -860 0 14 1
What are the parameters to adjust to have a TTE that decreases correctly if it is possible ?
It is possible to do better ? If yes how ?
Thanks and Best Regard
Stéphane