Hi Team,
I have a need to use the TPS26600 on a 24V power supply with the current limit set to 1.5 Amps. The downstream load that is connected enters a known high current spike 4 seconds after powered on.The load goes up to 1.8 Amps at 4 seconds after power up and then drops down to normal operation within 1 second.
I would like to use the TPS26600 so that the current limit is at 1.5 Amps. I need to adjust for a short period of time to allow the 1.8 Amp load to pass.
Do you all have a method to do so? Switching in a second ILIM resistor? Using a digital potentiometer? Using a DAC into ILIM?
Let me know your thoughts!
Thanks,