Other Parts Discussed in Thread: EV2400
I need to generate the new golden file of BQ20Z70 for the existing product by using EV2300.
The problem is that the USB windows driver of EV2300 is 32-bit only and my laptop PC has the 64-bit windows 10.
So the USB driver looks now working on my PC.
Here are the questions.
- Is there any available new USB driver of EV2300, which will work on 64-bit windows 10?
- I found the other option with EV2400.
- Can EV2400 be used to generate the golden file of BQ20Z70?
- If yes, can the generated file be used for the production with EV2300?