Hi,
The following information is listed in the "Current" column of the absolute maximum rating of datasheet P.5.
"Current on power pins (average current over 100k hour lifetime, Tj = 125°C"
Is this the specification of the average current value when operating 100 k or more at 125°C?
What is it when Tj = 100°C,108°C,110°C?
Best regards,
Yuto Sakai