This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LP87524B-Q1: LP87524B-Q1: make output stable when another output change the load current

Part Number: LP87524B-Q1

Tool/software: WEBENCH® Design Tools

Hi,

I use LP87524B-Q1 to change 5V input to multi-outputs, including 3.3V,2.3V and 1.8V.

The 2,3V is used for radio module. The radio module transmit per 300ms and when transmission, it need current change 0A to 0.9A and the current last about 15ms.

Because of the load change, the 2,3V voltage drops about 40mVpp per 300ms, which also make the 5V input of  LP87524B-Q1 drop and make the 1.8V output of LP87524B-Q1 also drop.

But the 1.8V output of  LP87524B-Q1 is used to ADC as reference and it can't drop when the 2.3V drop.

What can I do to make the 1.8V stable when the 2.3V drop because of the load current change?