This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS24750: TVS diode's replacement

Part Number: TPS24750


Dear Team,

In the TPS24750 reference design. D4 use [Diode, TVS, Uni, 18V, 600W, SMB SMB SMBJ18A-13-F Diodes Inc.]

Can they change to below components?

Please help on making sure these two TVS are suitable or not.

LOSC SMAJ18A  DIO TVS 400W 20-22.1V SMA-2P SMD

Diodes SMAJ18A-13-F  DIO TVS 400W 20-22.1V SMA-2P SMD

BR

Kevin