This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS26600-02EVM: Latch-off mode at 0.2A limit

Part Number: TPS26600-02EVM

Hi,

our customer tested Latch-off mode various current limit.

The customer complains that it will be Auto-retry only in the 0.2 A limit. Latch-off operation is performed with other current limit.

Why do you know that it will be Auto-retry only at 0.2 A?  Please let me know if you need confirmation.

This test follows the table below.  (http://www.tij.co.jp/jp/lit/ug/slvuav3a/slvuav3a.pdf)

Table 4 ,Page 4

J4      MODE     CH1 MODE selection
                         1-2 position sets latch-off mode

J5     ILIM         CH1 current limit setting
                         1-2 position sets 2.23 A    ... OK
                         3-4 position sets 1.5 A      ... OK
                         5-6 position sets 1 A         ... OK

                         7-8 position sets 0.2 A      ... fail (Auto retry operation)

They tested about U1( J4, J5). 

Best regards,

Hiroshi