Other Parts Discussed in Thread: BQ25700, BQ25703, BQ25713, BQ25703A
Hi Sir
May BQ25703/BQ25700 can support PD 3.0? (are there 2 part can support up to 20V/5A?)
May we have this kind reference design?
Bogey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Bogey,
The BQ25703A/700A can both support the power levels of USB PD and USB3.0. You may also consider the BQ25713/10 for the same application.
However, a host will need to change the input current limits charger to match the respective USB spec.
For a reference design, you can find several here in the product folder for the BQ25703A: 
Regards,
Joel H