Hi
I have used TPS548A20 for 1.8V, 10A output in one of my projects. In my initial design with an input voltage of 12V, the circuit works fine, providing continuous current upto 10A. But, while testing the same for a new requirement with an input voltage of 5V, i have observed that the output is oscillating (rather, switching between 0 and 1.8V)when the load current is above 5A and it is repeatable. Though webench suggests to use an inductor of half the value for the new design, I couldnt change it as it not in our inventory. I would like to know the reason for this. I have attached the schematic for reference.1.8V CONVERTER.PDF