Hello,
The data sheet shows that the signal RESET_IN is low or high active. where can you control that and in which default state is it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The data sheet shows that the signal RESET_IN is low or high active. where can you control that and in which default state is it?
Rekoe,
The RESET_IN polarity is OTP dependent. You can find the default OTP settings in the user guide: http://www.ti.com/lit/pdf/sliu011
For the TPS6590379, the default is active low. If you wanted to change the polarity, you could use the POLARITY_CTRL register to update the RESET_IN polarity. Note that any time the device is restarted, it will start in its default state (active low for RESET_IN). You would have to change the polarity each time the device turned on, after all the rails finished powering up.
Thanks,
Nastasha
>> The RESET_IN polarity is OTP dependent. You can find the default OTP settings in the user guide: http://www.ti.com/lit/pdf/sliu011
Thank you, the TPS6590379/TPS659037 has the OTP (Softwareversion) 0x97.
That has to follow that SMPS7 and SMPS9 are working.
I dont understand correctly the boot0/1 pin´s.
with boot0 I can select the generated voltage von SMPS3 between voltage level of 1,35V and 1,5V.
But what does boot1?
Hello,
Do I have to pull up Boot1 to use PMIC.RESET_OUT -> AM57xx.porz correctly?
I think independently of BOOT1, PMIC.RESET_OUT will toggle to high on power up sequence.
Will PMIC.RESET_OUT toogle with Boot1=high at the time of an warmreset event?
What about the difference between RESET_OUT and POWER_GOOD?
RESET_OUT will toggle to high if the power-up sequence has been completed. But are the voltage levels checked? What happens if one LDO has a fault like a short circuit?
Does PWGOOD just check voltage levels on the SMPS?
In my application I don't want to use any switches or buttons to reset / switch-on the devices. Are the following HW-settings correct?
- PWRON is floating
- RPWRON is floating
- nreswarm <- AM57xx.reset_out
- nsleep is floating
- boot1 = high; boot0 = low (because ddr3_lp is used)
- enable1 is floating
- gpio7 is pulled up
- gpio0..6 are pulled low
- pgood and reset_out are combined with a logical AND function
- RESET_OUT -> AM57xx.porz
Rekoe,
It is recommend that BOOT1 is pulled high for correctly generating a POR on the AM57xx devices. With BOOT1=1, RESET_OUT will toggle on power sequence and warm reset.
POWERGOOD will go high when SMPS12 goes high, and go low when SMPS12 goes low. You can configure POWERGOOD to monitor other SMPS rails too if desired. POWERGOOD does not monitor LDO voltages. RESET_OUT does not check the voltages. It goes high when specified in the power sequence. It will stay low if there is no ON request.
If a SHORT occurs on any rail, the rail affected will shut off. If the short is cleared, the rail will turn on with a POR or by reading the SHORT STATUS register.
I also recommend using Figure 3 of our user guide to verify your HW settings (http://www.ti.com/lit/pdf/sliu011). I recommend pulling NSLEEP up to VRTC. Also, GPIO7 (POWERGOOD) pulled high will have the device set in an always-on state. You should ensure you have a way to disable the device. TI doesn't recommend using loss of power to disable the PMIC since the power down sequence will not be correctly implemented.
Thanks,
Nastasha
Hello Nastasha,
thank you for your answer.
If I have connect the PMIC and processor like figure 3 on (http://www.ti.com/lit/pdf/sliu011) :
The NRESWARM is connected trough a voltage level converter with RSTOUTn from processor.
At the time on starting up the pmic, the processor is in reset. That has the consequence the the RSTOUTn (processor) is low and that signal is on PMIC NRESWARM.
Is the NRESWARM ignored while waiting for it to go high?