Other Parts Discussed in Thread: UCC28951, TINA-TI
Hello,
I am working on a design of 2kW DC-DC converter where the input is 380-400V DC and the required output is 150V. For this I would like to use UCC28950 Full Bridge Synchronous Rectifier. I would like to know if UCC28950 is a good choice for this kind of application. I used the SLUC222C, the Excel Design Tool for UCC28950 and came up with a solution. could you please let me know if I am doing it right. Please suggest if there is any mistake. I am not able to simulate the model in PSpice as the models for the mosfets mentioned below is not available Therefore, I have to design based on the excel design tool only. Therefore, I would like to get your expert opinion on this matter.
For Mosfets QE and QF, I have chosen the values from an Infineon Part - IPP110N20N3
For Mosfets QA, QB, QC and QD, the part selected is - IPW60R070CFD7
Regards,
SambuddhaUCC28950 Excel Design Tool_SLUC222C_140V_2kW.xlsxUCC28950 Excel Design Tool_SLUC222C_140V.xlsUCC28950 Excel Design Tool_SLUC222C_140V.xlsxInfineon-IPW60R070CFD7-DS-v02_00-EN.pdfUCC28950 Excel Design Tool_SLUC222C_140V.xls