Other Parts Discussed in Thread: BQ25895, BQ25898
Team,
a) I am looking for a charge with the following specification. Do we have something that could fit?
The system will be mostly power from the Vin source. The battery (Li-Ion 3,8V 800mA) will only provide power when the Vin is not present (ie for emergency in case of main power failure).
The electrical specs would be:
Vin (4.5Vmin/ 10Vmax)
Vout 3.8V
I out : 3A min / 6A max when power providing from the Vin
I out: 2A max when power provided from Battery (no power coming from Vin).
Do we have a device that will has a BUCK to regulate the output to 3.8V in both scenario (with Vin present or from battery)?
The ideal solution would be like BQ25890 but with an Output that could be regulated to 3.8V instead of 5V. Is it possible with some of our BQ2xxx devices?
b) What is the closest/cheapest equivalent to LTC4040 (http://www.analog.com/en/products/ltc4040.html ) we have?
Thanks in advance,
Anthony