Other Parts Discussed in Thread: BQ24074, BQ24073
Dear TI,
We are working on a design that uses the bq24070 to charge a single cell Li-Ion battery from a 5V 3A AC Adapter.
The idea of having an additional auxiliary pack with the same IC in it was thrown around and I'm wondering if that would work.
Essentially there would be another battery pack with a bq24070 in line with the existing one.
We think it would possibly work if the 5V AC Adapter is charging both packs.
However, without it, would the auxiliary pack's output (4.4V) be enough to power the existing pack with the bq24070 already in it?
Thanks in advance.
Best Regards,
Kevin Knicker