This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59116-Q1: I set the REXT,but output current doesn't change as datasheet described

Part Number: TLC59116-Q1


Dear TI Experts,

Now I am using TLC116-Q1 to drive 3 RGB, but I found green led is not as bright as red and blue led~

The current is about 20mA, I change REXT resistance from 720Ω to 360Ω, but led brightness is darkened

According to the  datasheet, the current should be higher, Can I know why?

PS:Now the PWM is set to max brightness,and output voltage is about 2.5V