Hi,
Since TI has hundreds of charger IC's. I need some help picking a suitable charger with the following specs:
Use-case:
- charging station for single-cell 4.2V Li-Po packs (<1000mAH size packs)
Requirements:
- Must work standalone, no need for i2c/cpu
- configurable charge current, in this application ~500mA for 1C
- configurable max-charge threshold, i.e. stop at 3.9V (related to shipping, the cells must not charge to 100%)
- led indication for charging vs done
Please advice!