This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: Transferring Learned Values with Golden Image

Part Number: BQ4050

Hi Team,

My customer is trying to generate their BQ4050 golden image, but would like to understand how to do it so that the learning cycle transfers and the correct Max Error is programmed. They currently cycle the golden pack and Max Error shows 2%, but it goes up to 100% when they read the srec since it resets the device. Is it possible to create a golden image with the learned parameters so that they don't have to cycle every pack? My understanding is that the BQ4050 supports this.

Thanks,

Antonio