Hi,
I have a few question regarding the best settings that provides the highest accuracy for my application and how to get this into serial production.
It is a non-removable battery for a UPS-like device and it is used in the following way:
- Most of the time it is in shut-down node if not in use.
- If it is in use it is mostly in charge or maintenance charge mode.
- Only in an emergency is the battery discharged. It is discharged at a power rate up-to 10-times the cell capacity but discharge does usually stop before the cells are fully discharged. The entire discharge cycle would take less than 10 minutes to empty. The CUV would in this case stop any further discharge by opening the FET.
- The battery is then either recharged straight away and/or put in shut-down mode for storage until next use.
This workflow does not give the gauge time to do measurements and update settings. some of them might even be lost during the extended shut-down period between deployments.
1. What would be the best gauging configuration to get the highest accuracy out of it?
The second question is how to "initialize" the Gauge on a new production unit after it has been programmed with the golden image. I have noticed that fully charge capacity and relative state of charge is only correct after perform a full discharge - wait 5h - charge - wait 2h - cycle, which is not practicabe for serial production. Also, the Cell-Balancing is not enabled until update status reaches 0x0E, which will most likely never happen during the normal usage as it is described above.
2. How should I configure the gauge so that it is ready for use after programming the golden image so it shows correct initial state of charge and has cell balancing already enabled?
Thanks for the help,
Fred