The TPS53667-based power solution we have used now finds that the system is very unstable and the damage rate is high after working for a period of time.
1)The damaged chips are in the singular position. We don't know if the samples are not enough. Now There are 9;
2) We have read the power chip through PMBUS and started to stop working when the temperature reaches 100 degrees Celsius, but many chips are burned out, and all the burned chips look the same as the burning position. I am looking for A burnt one that can be seen clearly
the Schematic is below.Can you help me to analyze and solve the problem?