I am trying to make a AC/DC LLC resonant converter with UCC29950. In a step, I am a bit confused. This is related about SUFG/SUFS and MDSEL/PSON pin configuration.
In the design, I used auxiliary transformer winding for supply. But I am not sure how should I configure these pins mentioned above. In current design, I left SUFG open circuit, SUFS is shorted rectified and regulated 15V supply which comes from auxiliary winding. MDSEL pin is also shorted to 15V.
Is there anything that I missed? For example, depletion mode MOSFET or external control signal for MDSEL pin is required?