This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM43603: LM43603 damaged

Part Number: LM43603

Hi  TIers:

I met a issue on charging board for the automotive, the LM43603 is used to convert the 12V to 5V for the external USB slave device. The schematic is below ,

The issue is that the LM43603 will be damaged during frequently plugging in/out the 12V input . The phenomenon of the failed sample is the SW to VIN, GND, VCC is shorted . And I also ask them to check the input voltage and output voltage when plugging in/out the power .

It indicated that there is under voltage on the VIN and Vout ,the lowest voltage of the 5V will be negative which could damage the chip.

So my question are : a)  That's the reason cause the chip damage when plugging in/out the power

                                   b) How to eliminate the bounce of input ?

Blue: 5V output 

Yellow: 12Vinput

SWPA6045 Series.pdf