This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM5088: How can LM5088 Current Limit be adjusted

Part Number: LM5088


Tool/software: WEBENCH® Design Tools

Hello,

I have to design a low cost Supercap charger board, and I'm considering using the LM5088MH-2 to charge them.

At TI's product page it is written that the current limit can be adjusted i wanted to simulate it with a current limit of 1A,

to not draw to much current  for the other parts.

But it doesen't worked my question is now how or if a current limit can be set so that the the maximum charging current is 1A.

  

Thanks in advanced

Alex