This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BUF16821-Q1: On recommended capacitor capacity of power supply pins (9 & 23 pins)

Part Number: BUF16821-Q1
Hellow,Expert.
I have a question about BUF16821-Q1.
In data sheet P25, 10 μF is recommended for the bypass capacitor of the power supply pins (9 pins, 23 pins).
Is it possible to change this capacitor to a smaller capacity?
Specifically, 4.7 μF, 2.2 μF, 1 μF capacitors are assumed.
Also, please let me know if there are problems that can occur by lowering the capacity.

Best,Regars.

Noriaki