This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563219: Maximum Duty of T

Part Number: TPS563219


Dear Team,

Datasheet mention, the recommended maximum duty cycle is 65%.

If my customer will operate at around 70%, is it okay?

input voltage:4.75, output voltage: 3.3V.

Best Regards

Kevin