I'm looking for a BMS chip which is capable of determining that one out of three cells has fails.
If this is detected the failed battery doesn't get used anymore and the BMS goes working on on two cells only.
I'm asking this because we have had battery packs where one of the 3 cells fails.
But it wouldn't be a problem for us if the BMS keeps on working but then with a lower output voltage.