This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28780: Turn off Over Power Protection

Part Number: UCC28780

Hello,

I am using UCC2870 for my Activ Clamp Flyback Converter and my goal i to make a Converter with a output power 160W (Vo=40V and Io=4A). I am Using your UCC28780 GaN SIMPLIS Model (45W Output Power) for my Simplis Simulation. I already changed the Parameters for the (Rvo1  and Rvo2) and it worked i got something about Vo=40V and Io=4.3 A but after 160ms of Simulation, the Over Power Protecion turns on and breaks up!

I tried to program it by changing the Values of Ropp and Rcs but it Didnt work. Can you please tell me which Parameters i need to change, to become a activ clamp Flyback Converter with Po=160W. And how i can Calculate that?

Thanks!

BR

Ivan