This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28700: Fuse tripping while using oscilloscope for primary side measurements and analysis

Part Number: UCC28700


Hi,

I have just designed a Flyback Power Supply using the UCC28700. The connector(power receptacle) for the AC mains contains just two terminals line and neutral no earth. The problem is whenever I connect my oscilloscope reference to the ground on the primary side the fuse for my office is tripped.

The input to the circuit is 230V 50Hz. I am using single ended 10:1 passive probes rated for 300V RMS for my measurements. Please let me know the best technique to observe the primary side waveforms for the circuit.

Thank you in advance.