Part Number: LM5060
Is there a way to increase the gate sourcing current of 24uA?
Is it sensible to drive an additional current (250uA) permanently into the gate to ensure faster switching? In off state this additional current will be handled by the LM5060 which is capable to sink 2.2mA and keeps the gate voltage low. Is the LM5060 able to permanently handle this additional current? A broken LM5060 will result into a gate current and into FET activation.