Other Parts Discussed in Thread: TPS61291, TPS61021A, TPS61099
HI,
We are looking for an ultra low power buck in order to charge a 1F supercapacitor at 3.6V, the system is powered by a 3.6V LiSOCl battery which can provide only limited current (10mA nominal, 30mA peak) our load is drawing 47 mA max for 11 second max (per 24h) rest of the time the MCU is only powering it internal RTC, the supercapacitor can accept voltage up to 5.5V and has no charging curent limit, thus the problematic is limiting the current drawn from battery during charging with best possble efficiency and eventually control the load switching during the 11 second duty period (not sure if it is really needed since the supercap can provide over 50mA and thus the battery shouldnt be sollicitated even with no load switching).
We need something similar to the TPS62740 with ultra lo Iq, 3.6V output (the TPS62740 output is 3.3V max ), current control and load switching.
The idea is to limit the load to the battery at 10mA or less when charging, avoid losses associated with a current limiting resistor, and eventually being able to switch load to supercapacitor only when the MCU enters it duty period and draw 47mA (via MCU gpio control), ideally we would like to avoid need for any MCU control during the charging, so that ithe MCU can stay in RTC standby mode everytime except during it 11 second duty.
Any suggestion will be very welcome