Other Parts Discussed in Thread: TPS23861,
Hi Darwin,
As per your feedback we have changed the optocoupler (FOD817A) and TL431A ,now we are getting 24V output fine.
But we have given two option type1 and type 2 by giving jumper setting option for classification resistor selection I.e 63.4ohm and 90.9 ohm.
we have TPS23861EVM PSE ,when we keeping our jumper at the 63.4ohm position it passes signature detection and classification ,but when we keeping at the 90.9ohm position it fails the signature,,Is it because PSE is type 2?
when we use the TYPE1 midspan PSE by keeping jumper at the 90.9 Position it fails to pass the signature detection.
Please tel us the reason for this signature failure?suggest more about this signature setting ,since both the type1 and Type 2 PD.
Note:our circuit draws about 200mA maximum at the output(24V/0.2mA) about 4.8W.
If it is 4.5W Output power it supposed to pass signature detection for type1 (90.9ohm) right?
Please suggest where we done wrong or how to solve this ?
Other than this signature issue converter is working fine.
Regards,
Namith