This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EV2400: Using the VCC pins on 4 pin header

Part Number: EV2400

Hello there,

I wanted to use the WOD.2 pin from J3 header in order to provide voltage for the I2C interface device connected thorugh J3 header. The problem is, there is no voltage on WOD.2 pin. tracing it on the schematic reveals that this output is controller by U12, which is driver using signal WOD.2EN by the EV2400 MCU. The datasheet states that those pins are for future use. Is there any real way I can turn the WOD.2EN at the moment using 0.18 firmware? Maybe there is a newer one? I would appreciate all help.