Dear Roberto,
How are you? Hope you doing well.
While going through the software programes for PMP8740 we have stucked at few things...
1) How the Fan speed set in program? what is 415 count ?
2) In software Port P2.7 is assigned as 'Connect Load' ; but in hardware we are not able to find this signal, As on Microcontroller board J1_pin5 is P2.7 but on full bridge board J2_pin5 left open. plz help.
3)Why there are difference between parameters range in Flash.c and main.c ? eg. tricke voltage 0-274 (In flash.c) & 0-315 (in main.C); mains UV 170-200 (In flash.c) & 80-200 (in main.C); current limit 10-60 (In flash.c) & 0-60 (in main.C); Minimum_current_tricke 2-10 (In flash.c) & 2-20 (in main.C)
4) when program starts we have Minimum_current_tricke range in main.c as 2 to 20 and if we set value as 19, then during operation Minimum_current_trickle value will be considered as 19 Only. But when charger unit is switched OFF and ON then while restoring the Minimum_current_tricke vlaue , it will restores as 6 as per flash.c. am i correct? If i am correct, then why it restores as 6 instead of 19? and if i am wrong then what value will be restores in Minimum_current_tricke? 6 or 19? plz help.
Thanks,
Anjana