Other Parts Discussed in Thread: TPS61165, TPS61169
I am currently using LM3410XSD (WSON | 6pin) to drive the backlight of a display on a controller. Unfortunately, the display is changing to one that requires 26V nominally at 60mA. The LM3410 max output voltage is 24V. Is there a footprint-compatible LED driver that would work in place of LM3410 so that I do not have to change the PCB? The requirements are as follows:
- Similar footprint as LM3410XSD
- Input voltage: 3.3V
- Output voltage: 30V max
- Current: 60mA max
It looks like TPS61165 is the closest match, but it seems that this device can't support 30V out with 3.3V in--is that true? If so, are there any other options to consider?
Thanks,
Brian Angiel