Other Parts Discussed in Thread: LM5176
Dear Specialists,
My customer is considering LM5175 and LM5176.
He has inquries about OVP spec.
I would be grateful if you could advise.
---
(1)Could you tell me the Min / Max value for the specification of the output overvoltage protection (OVP) function of the LM5175 and LM5176?
(2)If output overvoltage protection works, will all four switch FETs be stopped or which one of the four stops?
(3)How much delay time between detection of OVP and stop of FET?
(4)I'd like to use adjusting output voltage.
Is there a possibility of damage to FET and Rsense when the output voltage change from 24V to 12V.
When voltage change happened, OVP occur at that time, so is there a possibility of reverse current flow from output to low side FET.
Can LM5175 and LM5176 protect such condition?.
---
I appreciate your great help in advance.
Best regards,
Shinichi