This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510-G3: Procedure for repeat learning cycle to improve Qmax anx RaTable and how to improve the discharge result

Part Number: BQ27510-G3
Other Parts Discussed in Thread: GPCCHEM

Hello,

If we want to improve the ra table, is it a procedure to repeat learning cycle ?

For IT Enable, Update Status, .... between each cycle ?

I do the learning cycle and i see that the TTE doesnot follow a straight at the end of disharge.

What could be the cause ?

How to solve it if it is possible to do better ?

Is there something wrong during the configuration and the learning cycle

Please see the curve TTE at the end of discharge during learning cycle.

And the log file during the learning cycle.

Please find also the gg.csv file after the discharge during the learning cycle.

learning cycle 25092018.zip

Thanks for you help.

Stéphane