I'm a little confused about the phase of the clocking signals if two TPS50601-SP devices are configured to operate in a Master/Slave configuration using the SYNC signal to connect the two. This is to configure a dual phase converter.
With the RT pin floating, the master will clock at 500 kHz. Its SYNC output is inverted from the switching clock used in the Master.
Since the Slave device is configured to operate with an external clock being fed to its SYNC pin, does this clock get inverted internally in the slave? This would make the switching clock of the slave align with the switching clock of the master. This is the result we see in Pspice simulation.
To get the phases to be 180 deg out of phase, do i need to add an external inverter on the Slave's SYNC input?