This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS74801: TPS74801 3.3V output issue

Part Number: TPS74801

 Dear Sir,

I use TPS74801 to generate 3.3V , Vin is 5V. Rfbt = 3.57K, Rfbb = 1.15K, so the output should be 3.3V according to Vout = 0.8*(1+Rfbt/Rfbb)

the Vbias is connected with Vin together. Cin is 22uf, and Cout is also 22uf.

But the real Vout is about 3.8V, it is much bigger than 3.3V,

is there something wrong in my design?