Bq24104, when used for charging 2 li ion cells is not working. I connected the example design in the datasheet, apart from the inductor and output capacitor values (which are according to my design), every other component value is the same as that in the example circuit. when connected, the led connected to the stat 1 pin is blinking. I supplied the TS pin with voltage in the range of VLTF and VHTF again the same thing is happening. I would be much obliged for your response.
Regards
Zetamp