Hi TI,
Here are two application:
-- input: 5V output: 75V/25mA
-- input: 5V output: 200V/10mA
1. I have found LM3478 and LM5122, could you help to check if these are good for the request or not, or any better solution for this, thank you.
2. There is a TI design, PMP20183, using LM3481, is it possible to use LM3478 and LM5122 to replace?
C.T.