Other Parts Discussed in Thread: , EV2400, TPS23861, TPS23880, TPS2388
Hi,
i have a board with TPS2384 and a board with TPS23841 and want to access by gui "TPS2384 EVM" slvc078a.
I2C working is checked succesfully with bus-pirate, the device acknowledge the adress check.
The gui needs an EV2300. I bought the successor EV2400 because it is the working with Win7.
EV2400 (Firmware 0.18) is plugged in USB and all green LEDs are on, the powered target is connected at I2C Port2.
The EV2400 is detected as HID with HardwareID: HID\VID_0451&PID_0037&REV_0012 .
But there is still no data connection between running gui and the target.
"bq80xRW.ocx missed" in gui after installed sluc291.
What driver i need? Is the EV2400 working with gui "TPS2384 EVM"? Thank you in advance.