Dear all,
one of my AA is designing a Buck following the application info present in the datasheet.
Vin 24V, Vout 12V, Iout 300mA
The Buck has been tested connecting an active load and increasing the load current. As soon as the load current approaches 250mA the transistor stops switching and the device is damaged. After the damage the designer has measure 12ohm of resistance between CE pin of the output transistor.
Below the schematic.
Do you have any hints ? My idea is that the transistor does not have enought time to discharge itself.
regards,
Domenico