Other Parts Discussed in Thread: BQ25120A, BQ25150, BQ24201
Hi,
I am designing a new battery powered system to be used in high temperature environment and i am want to use Taridan's TLI batteries (which have extended temperature range) but these batteries have special charging conditions such as:
charging voltage: 4.1V
at normal temperature: Max charging current = 100mA
at high temperature: Max charginf current = 20mA
I have been digging in this forum and found that charging these batteries might be challenging so i would like to know if TI has some technical solution for charging these batteries taking in consideration these particular charging conditions.
In previous projects i've used the BQ24092 but this IC can't be used for charging these batterires (ISetMin = 100mA and has VO = 4.2v). Can you help me finding a solution for charging these kind of batteries?