This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92515-Q1: TPS92515-Q1 Design for Automotive 24VDC System

Part Number: TPS92515-Q1

Hi Support Team,

I have project use TPS92515-Q1 design for automotive 24VDC system.

Consider Load Dump, How do I chose input cap and TVS spec?   if you had designed experience, please advise me, thanks!

  • Hello John,

    First you need to know what the load dump specification is. This includes voltage and possible current to figure out if it can be clamped or if it has to survive the load dump voltage at high current. The capacitor should be sized to be able to handle the load dump voltage or clamped input voltage.

    BR,