Other Parts Discussed in Thread: LM5110
Hi,
I am looking for a half bridge gate driver with the possibility of negative bias. I am thinking of something like a combination of UCC20520 and LM5110. Is there a part available, which suits my requirements? Currently I am using the LM5110 but unfortunately I have a lot of ringing on the outputs of the driver which causes distortions on the output of the half bridge at short on times. I am hoping that a part similar to UCC20520 provides more stable outputs.
For further specification here are some details about my requirements:
- ton = 20ns – 20µs
- toff = 500µs – 1ms
- duty cycle min = 0.002%
- duty cycle max = 4%
- Vvarneg = -1.5V – -5V
The reason why I need negative bias is due to the negative voltage across the half bridge I need a negative voltage to fully turn on the FET. For further information I have attached a simplified schematic.