Hi,
I have designed a battery charging circuit around BQ25713 considering following power requirement
Output power (load): 4.2V, 8A
A battery specification: 1S8P (20AH @ 4.2V nominal voltage).
Charging current: 1A (when charging the battery load will take 6.5-7A current.)
While designing I have took reference from EVK SLUUBT8A.pdf document. Please find attached PDF.
I have a queries as below:
1) ILIM_HIZ pin: As per equation I have calculated voltage for the pin and it is coming 4.2V (1 + 40 x 8 x 0.01 ). Pl verify the value of R666 & R667.
2) Is it required to put input protection circuit containing Q73 and Q74? What impact it will have if I directly provide source supply to IC?
3) In my design I do not have USB charging application, so it is not required to provide power in the reverese direction to VBUS. While on backup battery will constantly give supply to VSYS_4V2 rail only.
Also, please do overall review and provide your comments if anything missing.