This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: Excessive temperature

Part Number: LM5175
Other Parts Discussed in Thread: LM5176

We have exactly this behavior that the controller temperature is already above 65 ° C without load. The problem is that of about 200 assemblies that are already manufactured, only about 10% show this behavior. The others are at least 30 ° C cooler.

An idea where to look?

What was the problem solution in the previously curtailed project?