Customer design a 30V/20A charger circuit with bq24640 for special/Sport electrical Car application.
1. ISET problem (ISET pin's Voltage is not stable and goes up)
- During heavy load, the voltage at ISET pin can go up from 0.899V (no load) to 1.01V (20A load) around.
a. Customer tried to add a 0.1uF between the VR resistor, however, the problem is NOT gone!
b. Customer tried to supply ISET pin voltage by external power supply, however the power supply voltage goes up also!
Is this normal behavior? if not so, why and how to improve it? Customer already implement bq device on the board and urgent to offer the goldern sample to end-customer. pls help on this issue.
2. Can bq24640 support up to 20A charging current?
3. The VCC pin of the bq24640 is connected to the Flyback Aux power of 30V,typ? The application input voltage is 28.5V to 32V aound, and the output voltage is designed to 29.3 around.
In the Recommandation Operating conditions, it says the SRP and SRN need to work with voltage less than 28V. So is this application suitable with bq24640?
Pls advice. thanks.