This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51367: About variation of operating frequency

Part Number: TPS51367


Hi,

I have created a circuit using the TPS51367 device.
Now I am checking the operation of the circuit, but there is concern that the operation of TPS51367 will affect other devices.
It is mainly concerning operating frequency.
I understand that TPS51367 performs DCAP2 control, so the operating frequency varies to some extent.
We know that the operating frequency is not regulated by electrical characteristics.
Still, I would like to check the variation in operating frequency and the temperature characteristics.
Can you tell me how much variation in operating frequency is assumed in my specification over the whole temperature range? There is no need to guarantee this.

(specification)
Input voltage: 6 V to 9 V
Output voltage: 1.0 V
Output current: 1.5 A to 3.5 A
MODE pin: GND connection (fsw = 400 kHz)

Best regards,